2019-04-02 11:05 PM
2019-04-02 11:30 PM
I've seen some of these. Could be many causes. I won't touch on reasons though.
When it occurred for me it was pretty reproducible, and mostly successful after closing any apps that could hold a lock. I'm Windows, so included Windows Explorer too.
You might learn something from its log. In Windows it's at C:\Users\<username>\.stm32cubemx.
2019-04-03 12:12 AM
Hello alister.
I closed every folder and explore. But it is useless.
And I removed STM32CUBEMX and reinstall but the same issue is happened.
Do you have another idea?
Maybe I will ask the engineer making STM32CUBEMX.
2019-04-03 3:18 PM
What errors are flagged in the log?
2019-04-28 10:06 PM
Below log is the file "./stm32cubemx/ STM32CubeMX"
I really wonder how do I fix it.
2019-04-25 14:55:56,913 [INFO] ProjectBuilder:1489 - Time for Copy HAL[0] : 456mS.
2019-04-25 14:55:52,479 [INFO] CodeEngine:190 - oldGeneratedFile, D:\AProject_2018\19)Lucis\code\Lucis_Ethernet\Inc\stm32f4xx_hal_conf.h_save
2019-04-25 14:55:52,911 [INFO] CodeEngine:208 - Generated code: D:\AProject_2018\19)Lucis\code\Lucis_Ethernet\Inc\stm32f4xx_hal_conf.h
2019-04-29 1:50 AM
They're not errors. I won't be able to help as I don't have its source and can only guess.
> Maybe I will ask the engineer making STM32CUBEMX.
Please share what you learn.
2019-04-29 2:28 AM
Hello, Alister
If I make the follow directory "D:\Project_2019\19)Lucis\code", the stm32cubemx emulation is stoped while making ewarm project file.
but if make the follow directory "D:\Project_2019\Lucis_choi", the file is generated succefully however the file is not good(compile error is happened)
I attached the file.
==> Pherhaps the jave affect the stm32cubemx, I recover the window os as default set.
But it is useless, the symptom is same.
I rellay wonder which one is wrong
========================
" Circumstances"
CPU : STM32F407VGT
Only set : ETH with MII, LWIP
clock is defulat set
compiler : EWARM V7
stm32cubemx version : 5.2.0
========================
2019-04-29 3:35 PM
> the file is not good(compile error is happened). I attached the file.
I wasn't excited that you'd attached the entire project. Better if you'd posted only the error message. Anyway I downloaded it and it builds fine for me. Your IAR is an earlier version as it said its project was an old format and would I like to convert it. Mine is V8.32.3.
> If I make the follow directory "D:\Project_2019\19)Lucis\code"
Don't do this. STM32CubeMX has many more important problems to fix than this.
2019-05-02 11:53 PM
Thank you Alister,
I changed compiler as you mentioned. I forgive up the fix the bug. ^^
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.