2023-07-24 10:57 AM - edited 2023-07-24 12:32 PM
When will STM32CubeU5 have an example OTG_HS CDC_Standalone application? I've use the example CDC_Standalone app from the many other STM32Cubes, but the M33 core appears to have a few significant differences. Banging my head on the wall.
That is, STM32CubeU5\Projects\STM32U5x9J-DK\Applications\USB_Device\CDC_Standalone
2023-08-03 7:27 AM
Hi @BillyBob ,
Examples in the STM32CubeU5 package are based on USBX.
For Customers who need to use the legacy library, ST provides the STM32U5 Classic Core Middleware (CoreMW) MCU Firmware Package.
I assume that you will find what you need there.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-14 10:43 AM - edited 2023-08-14 11:53 AM
Thank you Amel, but it's still not giving me what I need. Every CDC_Standalone example project I've reviewed, including the stm32u5-classic-coremw-apps example, use the OTG_FS peripheral. We are using the STM32U59A MCU which only has an OTG_HS peripheral.
It's certainly possible I've overlooked something, but I believe I've configured the RCC, SYSCFG, and OTG_HS peripherals correctly. The dev kit's USB-C still does not enumerate.
Any ideas are much appreciated.
2023-09-05 1:27 AM
Hi @BillyBob , Just to make sure I understand the situation:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.