cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in X-Cube-AZRTOS-H7 V3.3.0

Intector
Senior

Hello STM-Team,

I'm working on my project with an STM32H723ZG and ran into an issue with the code generation when I selected "Network Interfaces" in the  AZRTOS configuration.

Intector_1-1733095953265.png

The code generation will add "NX_ETH_INTERFACE_ENABLED" to the "RTE_Components.h" but forget the "#define" in front of it.

Intector_2-1733096278529.png

 

That is somewhat annoying because I have to manually add this everytime I regenerate the code.

 

 

 

1 REPLY 1
STTwo-32
ST Employee

Hello @Intector 

Thank you so much for sharing this input. I'm able to reproduce this behavior and I've escalated for correction on the coming releases (under internal ticket number 197441).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.