2016-09-25 10:16 PM
Hello,
I used STM32CubeMX with 4.16.0 or 4.16.1 version.below situation :''STM32Cube Firmware Library Package'' option is ''Add necessary library files as reference in the toolchain project configuration file''IAR's error message is all same belowFatal Error[Pe1696]: cannot open source file ''D:\Work\IAR_WORK\ARM\Projects\ZNC-514B_3MCU-S1\EWARM\D:\Temp\
STM32CubeMx\STM32Cube_FW_F7_V1.4.0\Middlewares\Third_Party\FreeRTOS\Source\timers.c''
So, IAR cannot find Driver files(HAL_Driver's files)Because included wrong path for Driver files.- �Toolchain Folder Location� is
D:\Work\IAR_WORK\ARM\Projects\ZNC-514B_3MCU-S1\EWARM\
-�
Repository Folder
� isD:\Temp\STM32CubeMx\STM32Cube_FW_F7_V1.4.0\Middlewares\Third_Party\FreeRTOS\Source\timers.c
2016-11-30 6:18 AM
Hello
I have just checkd with the new cubeMX 4.18. The problem seems to be solved. Reagrds A.B.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.