cancel
Showing results for 
Search instead for 
Did you mean: 

Break at address 0x18003A1A with no debug information in CubeMX-generated project

MownishBugatha
Associate III

MownishBugatha_0-1770187275194.png

I generated a project using STM32CubeMX for the STM32N6570-DK board.

Steps performed:

  1. Generated code using CubeMX (default configuration)

  2. Imported project into STM32CubeIDE

  3. Built the project successfully (no build errors)

  4. Attempted to run/debug the application

During programming / start of execution, the debugger stops with the following message:

Break at address “0x18003A1A” with no debug information available, or outside of program code

1 REPLY 1
Imen.D
ST Employee

Hello @MownishBugatha 

Please provide more details (CubeMx and firmware version used) , which project used. If possible, share your ioc file.

How to write your question to maximize your chances to find a solution

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.