2024-10-09 6:19 PM
Hi i'm using MCU : STM32H743ZGT.
At several ADC documents, it says that when ADC1 and ADC2 end sampling, the two results are stored in ADC_CDR together.
The top 16 bits are the result of ADC2, or slave ADC, and the bottom 16 bits are the result of ADC1, or master ADC.
I want to know how the two ADCs are stored in different registers, for example, each ADC_DR.
Because I want to get more than 16 bits of data.
Of course, we use the two ADCs as dual mode.
Is there any other way?
Thank you.
Solved! Go to Solution.
2024-10-11 9:29 AM
Hello @giwonKIM ,
According to the internal feedback, ADC values are also stored in ADC_DR register in DUAL mode for both ADCs.
2024-10-10 8:48 AM - edited 2024-10-10 9:01 AM
Hello @giwonKIM ,
I'm checking internally and get back to you as soon as I have a feedback.
Internal ticket number for tracking 193439.
Thank you for your patience.
2024-10-10 11:04 AM
I see in Reference manual RM0433 Rev 6, ADC section, p. 1029:
Bits 15:14 DAMDF[1:0]: Dual ADC Mode Data Format
This bit-field is set and cleared by software. It specifies the data format in the common data
register ADCx_CDR.
00: Dual ADC mode without data packing (ADCx_CDR and ADCx_CDR2 registers not used).
01: Reserved.
10: Data formatting mode for 32 down to 10-bit resolution
11: Data formatting mode for 8-bit resolution
Register: ADC x common control register (ADCx_CCR) (x=1/2 or 3)
Example: page 981
Interleaved dual mode: a DMA request is generated each time a new 32-bit data is
available:
1st DMA request: ADCx_CDR2[31:0] = MST_ADC_DR[31:0]
2nd DMA request: ADCx_CDR2[31:0] = SLV_ADC_DR[31:0]
And I see HAL can configure DAMDF bits:
MODIFY_REG(tmpADC_Common->CCR, ADC_CCR_DAMDF, multimode->DualModeData);
2024-10-11 9:29 AM
Hello @giwonKIM ,
According to the internal feedback, ADC values are also stored in ADC_DR register in DUAL mode for both ADCs.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.