2023-08-06 3:24 PM
I am having problem with FATFS remounting with Cube IDE and STM327H50. Tracing the program surfaced the SD_initialize() function which is defined in the ST library file FATFS/Target/sd_diskio.c.
The problem is that when BSP_SD_Init() failed, SD_initialize() returns whatever value previous functions left in the variable Stat, which can cause SD_initialize() to sometimes return OK even if BSP_SD_Init() failed.
Am I missing something?
/**
* @brief Initializes a Drive
* @PAram lun : not used
* @retval DSTATUS: Operation status
*/
DSTATUS SD_initialize(BYTE lun)
{
#if !defined(DISABLE_SD_INIT)
if(BSP_SD_Init() == MSD_OK)
{
Stat = SD_CheckStatus(lun);
}
#else
Stat = SD_CheckStatus(lun);
#endif
return Stat;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.