2021-02-16 9:55 AM
After I tried to clone in suggested 3 steps, one of which was to modify new project name in project.c file I got the same name of .ioc file and error in .s startup file?
Sorry, I was wrong, according to suggesting I should edit with the new name
.project file not .cproject.
After I corrected my mistake and edited .project file I still got old name in .ioc
file which didn't work in new project.
========================================================
Steps to Clone STM32CUBE projects.
2021-02-16 2:26 PM
If STM32CubeIDE even more obvious let's rely too on File > New > STM32 Project from an existing STM32CubeMX configuration file (.ioc)
Result should be same. Then I would not call such as a clone procedure. All such is cloning project basis (device configuration, project structure, part of setup) but lacking end user code and end user setups if some. Not a big deal I agree to perform some copy paste to complete cloning work then.
All such can be useful.
2021-02-23 6:54 AM
The Project Explorer has 'Copy' and 'Paste' - that can be used to duplicate a project...
2021-02-23 7:20 AM
> After I corrected my mistake and edited .project file I still got old name in .ioc
Well so edit the .ioc too. Not all CubeIDE projects are based on .ioc.
The Eclipse part of CubeIDE is not aware of the .ioc file after generation of the project.
-- pa
2021-03-01 11:35 AM
I was happy to see this topic, but it was short lived. What if you want to clone one of the examples or demos? Few, if any, of which have even have .ioc files. Then you will have problems. In that case it is a matter of copying the individual files. You can copy the project, but you can't paste it, and you absolutely cannot "Save As", according to my version 1.5.1. It sure would have saved me a lot of copy/paste time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.