2023-12-04 12:31 PM
Hello,
i'm using cmake to build complete STM32F7 application. I was very happy to see cmake files in x-cube-azrtos-f7. The threadx, netxduo, and filex libraries themselves build find with cmake. The problem is when I am building the example project fo NxWebServer using cmake, it can't find a header file in nextduo/common/drivers/inc, since the cmake file for netxduo/common doesn't add this as a include directory. The IDE (eclipse-based) project in the example project builds fine, since the include directory is the project list.
https://github.com/STMicroelectronics/x-cube-azrtos-f7/tree/main/Middlewares/ST/netxduo/common
I opened issue in github but any advice welcome ahead of time.
https://github.com/STMicroelectronics/x-cube-azrtos-f7/issues/2
2023-12-04 12:33 PM
# ThreadX library
set(THREADX_ARCH cortex_m7)
set(THREADX_TOOLCHAIN gnu)
# specify out of tree source build so each library can pickup the user variables (i.e. *_USER_FILE)
add_subdirectory(${CMAKE_SOURCE_DIR}/x-cube-azrtos-f7/Middlewares/ST/threadx example_app_threadx)
add_subdirectory(${CMAKE_SOURCE_DIR}/x-cube-azrtos-f7/Middlewares/ST/netxduo example_app_netxduo )
add_subdirectory(${CMAKE_SOURCE_DIR}/x-cube-azrtos-f7/Middlewares/ST/filex example_app_filex)
################## PROJECT SETUP ######################################
project(stm32f769i-eval_app C ASM)
message(STATUS "CMAKE_EXECUTABLE_SUFFIX ${CMAKE_EXECUTABLE_SUFFIX}")
add_executable(${PROJECT_NAME} ${PROJECT_SOURCES})
target_link_libraries (${PROJECT_NAME}
stm32f7_hal
STM32F769I_EVAL
Comp-mfxstm32l152
threadx
netxduo
filex )
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.