2024-11-21 4:41 PM - edited 2024-11-21 4:42 PM
I have the latest and greatest CubeIDE v1.16t.1, confirmed with recent attempts to upgrade it. Recently I have been experimenting with the ultra librarian tool output in the IOC editor, which looks to be extremely useful. I have a project that uses an STM32F401RBTX, it was created by an earlier version of CubeIDE, but upgraded when I opened it.
I use KiCAD 5, and have been able to successfully create a symbol on a different project. However, the symbol that it creates for this one has two errors: first the pins are all located on top of each other, and second the poly lines have fractional positioning data that is rejected by the symbol parser. I have attempted to text edit out the fractions, but the pins appear to be stuck together and any attempt to relocate them with the symbol editor fails.
I cannot find any information about how to configure the librarian, is there an update or fix for this? Generated zip file is attached.
2024-11-25 7:21 AM
Hello @divmstr
First let me thank you for posting.
This is a known issue that has been tracked by the ticket number 196222
I will keep you posted with updates.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-25 9:20 AM
Thanks. Is there any work-around? I tried a different project with an STM32F723, and it worked. (Except the symbol was rather large...)
Cheers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.