2023-06-23 6:37 AM - edited 2023-06-23 6:40 AM
Hey there,
currently I am struggeling with capturing the sensor value from an si115x (Proximity & ambient light) Sensor.
So far, this would be my code:
void ReadSensorData(void)
{
uint8_t sensorAddress = 0x53 << 1; // shift left to account for R/W bit
uint8_t readProximity = 0x11;
HAL_I2C_Master_Transmit(&hi2c1, sensorAddress, &readProximity , 1, HAL_MAX_DELAY);
HAL_Delay(20);
uint8_t rawData[2]; // raw data is unreadable by itself, needs 16 bits see below
HAL_I2C_Master_Receive(&hi2c1, sensorAddress , rawData, 2, HAL_MAX_DELAY);
uint16_t rh = (rawData[0] * 256 + rawData[1])/3;
proximity=rh;
}
Instead of data captured by the sensor, I only get 4010. --> The Funciton void ReadSensorData(void) is called by a separate Task.
In another Task, the captured value is output via UART.
The value does not change, whatever I do...
I hope, that you could give me some advice.
Thanks in advance!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.