2025-09-11 1:09 PM
Hi, I use lasted available library’s and software Cube IDE and stm32f103 mcu. I create clear project with minimum required parameters for use usb MSD or COM, with using USB HAL, So I compile it and connect usb, device recognised and OS propose format it, all works correctly.
So the problem: if in settings project optimisation select any type not include “none” after programing device not recognised by OS if I connect it by usb. No meter what optimization level i select. In debug mode initialisation comes without return error, (OS still not recognized usb device)
Solved! Go to Solution.
2025-09-12 1:43 AM
so I find solution, in file usbd_desc.c in function Get_SerialNum(void)
need to assign values to variables or make it volatile and it fix problem
2025-09-12 1:25 AM
Hello @MichaelQuant
This issue is typically caused by compiler optimizations affecting timing, variable access, or interrupt handling—especially if shared variables are not declared as volatile. To resolve this, ensure all variables shared between main code and interrupts are declared volatile, check that all variables are properly initialized. You can also set optimization to -O0 specifically for USB-related files (like usb_device.c and usbd_core.c) while keeping the rest of the project optimized. These steps should help maintain USB functionality across all optimization levels.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-12 1:43 AM
so I find solution, in file usbd_desc.c in function Get_SerialNum(void)
need to assign values to variables or make it volatile and it fix problem
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.