2020-11-09 9:15 PM
hello
i use stm32cubeide 1.4.0 and cube programmer 2.5.0
i want to st link gdb server
https://community.st.com/s/question/0D50X0000BD4BDRSQ3/error-failed-to-erase-memory
The same symptom appears even if option byte is set and flash is deleted.
The above and symptoms are the same.
I know the solution. About this problem.
The solution was I copied the stld file inside the stlink folder and the problem went away.
Looks like a patch is needed from ST.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.