2019-05-07 11:47 PM
Hi everyone. I run STM32CubeIDE on Windows 10, and when I try to save STM32Cube project in the Device Configuration Tool with code generation after saving ("Do code generation on *.ioc file save" is checked), code generation fails (see screenshot). But when I press "Generate code" button at the toolbar or press Alt+K, code generation is OK.
It seems to be not critical, but a little annoying bug.
2019-05-08 3:44 AM
Oh my Generate Code button is always greyed out so I use Build All which still generates an .elf. And Alt-K doesn't work.
Anybody any ideas what I have to do to get it to ungrey ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.