2025-12-27 9:48 AM
Hello,
I'm facing very strange issues with STM32CubeIDE 2.0.0 under Linux Debian Trixie/Forky.
I'm running Kernel 6.17.11+deb14-amd64 with Plasma 6.5.4, KDE Framework 6.20.0 and QT version 6.9.2 in Wayland.
First issue is with debugger. I can start the firmware in debugging mode, runs but after few "Step Into" and "Step Over" commands the debugger is getting stuck. I doesn't take any commands anymore.
If I use "Restart" or "Terminate" or "Terminate and Relaunch" is starting again and again I can use few times "Step Into" and "Step Over"
Second issue is with windows ordering after using for a while STM32CubeIDE: it breaks completely the windows orders under Plasma and the only solution is to logout and login back and restart all apps.
I didn't get this issue with any other apps, except STM32CubeIDE.
2025-12-27 11:12 AM - edited 2025-12-27 11:39 AM
Hi,
i run LinuxMX , Debian system also, Xfce desktop, but i had no success with the Debian version, the generic version working.
Is still IDE 1.18.1 , and needed change to the GDB multiarch , the GDB didnt work (missing old libs).
So if you wanna try: install generic version...and check it.
2026-01-02 4:34 AM
For me I was able to install the packages.
I'm using the CubeIDE GCC version 13 and 14. Both of them have the same behavior.
I will try to check if the OS GCC for ARM is working better.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.