2022-08-23 11:23 PM
I have installed the stm32cube IDE 1.10.1 on ubuntu 20.04 using the appropriate installer package. Upon full installation when I tried to update the IDE using "check for updates" option in help, I am consistently getting the following update error message:
(attachment 1/2)
Other default repository URLs for CDT and core eclipse etc are working fine. I am behind a proxy and have configured the proxy settings too.
All default URLs are as follows:
(attachment 1/2)
Hope all this information is useful for resolution of the reported anomaly.
Regards
Sourabh
2022-08-24 6:55 AM
Hello @Moitra
I could not reproduce the issue from my side.
Did you try again the update. Maybe it was a temporary problem with the servers.
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-24 10:15 PM
Thanks Semer for the prompt response on the query. After your confirmation, I see that it is the problem of my proxy. I am setting the proxy parameters in the Preferences->general->network connections. Is there any other way I can set the proxy parameters for the repository update to work in my case ???
With best regards
Sourabh Moitra
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.