2020-10-14 3:12 PM
When I use .ioc file to generate the codes, it delete the entire project folder (include git information). Looks like I lose all the commits I haven't pushed to github. WTH is that.
Solved! Go to Solution.
2020-10-14 4:31 PM
There was an unfortunate bug in 1.4.0 that caused files to get deleted in certain cases. Might try updating to 1.4.2 to see if it's fixed.
2020-10-14 4:31 PM
There was an unfortunate bug in 1.4.0 that caused files to get deleted in certain cases. Might try updating to 1.4.2 to see if it's fixed.
2020-10-19 10:36 AM
Hello @LW.2ei ,
This issue is fixed in the STM32CubeIDE v1.4.2, as mentionned in the STM32CubeIDE release note.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.