2023-06-30 12:35 AM
How to use timer interrupt in GPIO interrupt
2023-06-30 12:43 AM
Priority?
2023-06-30 1:45 AM
Timer
2023-06-30 3:15 AM
Why ?
2023-06-30 4:23 AM
primary your personal sended code nobody see then nobody help.
volatile uint8_t count = 0; HAL_GPIO_TogglePin(GPIOB, Red_Led_Pin);
HAL_Delay(100);For ISR variables need volatile. Your count++ and if else is litle complicated.
And your code isnt timer interrupt in GPIO. You only start timer with IT method aplied...
HAL_TIM_Base_Start_IT(&htim3);And use Delay in callback is mistake if systick isnt higher priority code hang here
2023-06-30 5:21 AM
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, Green_Led_Pin|Red_Led_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : Push_Button_Pin */
GPIO_InitStruct.Pin = Push_Button_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(Push_Button_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : Green_Led_Pin Red_Led_Pin */
GPIO_InitStruct.Pin = Green_Led_Pin|Red_Led_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2023-06-30 5:27 AM
If I press the user button for 2 sec. Then red led will tern on .... Again I press button then red led will tern off.....If I continue press the button led will be tern off........
I did some changes but my problem is not solved ...
2023-06-30 6:07 AM
Dude, tell the people what you want to achieve.
Even your starting post "How to use timer interrupt in GPIO interrupt" is ridiculous, we have no time for guessing.
2023-06-30 6:41 AM
Extremely Sorry ... next time definitely I will try
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.