2021-08-11 8:09 AM
I am using NUCLEO-H743ZI2 with freeRTOS CMSIS V2. I would like to view freertos task list. I followed the instruction in UM2609, I did all of the modification, but I still can't trace freertos task list. When I start program, FreeRTOS task list is empty, I need suspend program, freertos task list is filled but run time shows n/a, stack usage shows n/a, after I resume the program, taks list is not updated.
Does anybody know how to fix it?
2021-08-12 12:34 PM
after one day works, I fixed the issue. I need set extra timer but faster than syc clock tick time, so I set 100Khz timer, then add the following code in main():
volatile unsigned long ulHighFrequencyTimerTicks;
//extern void initialise_monitor_handles(void);
void configureTimerForRunTimeStats(void) {
ulHighFrequencyTimerTicks = 0;
HAL_TIM_Base_Start_IT(&htim13);
}
unsigned long getRunTimeCounterValue(void) {
return ulHighFrequencyTimerTicks;
}
also add ulHighFrequencyTimerTicks++ in timer interrupt irqhandler.
it works every time you hit button "suspend" when program is running. the task list inforamtion will be updated.
2021-08-12 12:34 PM
one more, question is
is it possible to update task list information without suspending program running?
thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.