2019-12-07 4:19 AM
make clean
Cannot run program "make": Launching failed
Error: Program "make" not found in PATH
PATH=[C:/ST/STM32CubeIDE_1.1.0/STM32CubeIDE/jre/bin/server;C:/ST/STM32CubeIDE_1.1.0/STM32CubeIDE/jre/bin;C:/ST/STM32CubeIDE_1.1.0/STM32CubeIDE/jre/lib/amd64;C:\ProgramData\Oracle\Java\javapath;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Windows\System32\OpenSSH\;C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility;C:\Users\vip49\AppData\Local\Microsoft\WindowsApps;;C:\Program Files (x86)\ESTsoft\ALSee\x64;C:\Program Files (x86)\Java\jre1.8.0_151\bin;C:\ST\STM32CubeIDE_1.1.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.ide_1.1.0.201910081157\resources\project_importer\windows;]
21:14:13 Build Failed. 1 errors, 0 warnings. (took 82ms)
**** Build of configuration Debug for project MRM-IAP ****
Nothing to build for project MRM-IAP
2019-12-07 4:49 AM
OS likely intolerant of the wrong slash being used for directories.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.