2023-03-16 6:57 AM
Hi, I am running the vscode extension on ubuntu 22.04, and am getting the following error when trying to start a debugging session: "Could not find the path to "ST-Link_gdbserver". Ensure STM32CubeIDE is installed.". I have tried reinstalling the latest version of STM32CubeIDE but nothing changed. I have installed all the required programs (CubeMX, CubeCLT, MCUFinder).
The error prompt gives you a button to edit the launch.json to change the debug configuration, but i'm not sure what I'm supposed to change in order to get it to work. Thanks.
Solved! Go to Solution.
2023-03-16 8:25 AM
When starting the debugger it can happen the connection to the board fails with a Visual Studio Code message reporting "Unable to start debugging. No process is associated with this object."
The root cause can be identified in the DEBUG CONSOLE. Most probably the following message is reported: "Error in initializing ST-LINK device. Reason: ST-LINK firmware upgrade required."
To overcome the issue please install and run STM32CubeProg to upgrade the ST-LINK firmware as required.
2023-03-16 8:04 AM
Hi @JRobb.2
you would have to add the actual gbdserver path on your system to launch.json
2023-03-16 8:13 AM
Hi, thanks for the quick reply. However if I knew how to do that I wouldn't be asking this question hehe. So I would need to edit debugServerPath I assume? or is it miDebuggerPath? Also where should I look for the gdbserver? I have cubeIDE installed in its default location, so would it be in /opt/st/stm32cubeide_1.12.0/plugins/ ? Which folder/file should I be looking for? Thanks.
2023-03-16 8:20 AM
Ok, I think I have found the gdbserver executable at "/opt/st/stm32cubeide_1.12.0/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.linux64_2.0.500.202301161003/tools/bin/ST-LINK_gdbserver". I have changed "debugServerPath" in the launch.json to this value, but now I just get the error "Unable to start debugging. No process is associated with this object." instead. Any ideas?
2023-03-16 8:25 AM
When starting the debugger it can happen the connection to the board fails with a Visual Studio Code message reporting "Unable to start debugging. No process is associated with this object."
The root cause can be identified in the DEBUG CONSOLE. Most probably the following message is reported: "Error in initializing ST-LINK device. Reason: ST-LINK firmware upgrade required."
To overcome the issue please install and run STM32CubeProg to upgrade the ST-LINK firmware as required.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.