2020-03-16 11:48 PM
Hello,
I am studyng (first time) PWM using a Nucleo_401RE, STMCubeIDE, and HAL drivers;
I write some example using interrupt TIM2 and its TIM2_CH1 and PA5 to control the green led LD2.
The counter count UP, in the TIM2_IRQHandler , for the moment , I do nothing.
The signal is correct, but I have some question about HAL_TIM_OC_Start_IT and HAL_TIM_PWM_Start_IT , the first is:
where read complete documents about this Hal functions?
The user manual UM1725 say:
HAL_TIM_PWM_Start_IT
Starts the PWM signal generation in interrupt mode. (Very interesting)
HAL_TIM_OC_Start_IT
Starts the TIM Output Compare signal generation in interrupt mode. (Ah! interesting)
Why I ask this?
I want use a call back due to the interrupt call;the STMCubeIDE in NVIC have only one kind of interrupt: TIM2 global interrupt
I SUPPOSE that some differernts call back are possible only in base of the type of ____start, but what?
The famous UM1725 say, for example:
HAL_TIM_PeriodElapsedCallback
Period elapsed callback in non blocking mode. (Very interesting ...)
In details:
I want have DIFFERENTS call back when counter reach CCR and when when counter reload from ARR (I SUPPOSE there are two different IRQ calls) ;
Or recognize the two moments.
I have tryed different combination of kind of ____start and kind of call back: No valid results.
Many thanks and excuse for my english, but after Brexit ...
Luciano
2020-03-17 12:47 AM
> I SUPPOSE there are two different IRQ calls
In most of the timers, no. TIM1 is the notable exception (still merging some/many of the interrupts, and adding interrupts from other timers, at times; and maybe partially TIM8. Read the interrupt chapter in Reference Manual (RM).
> Or recognize the two moments.
You normally distinguish them (or, better, react to any of them) by reading TIMx_SR in the ISR. Note that you have to clear it (Cube/HAL does this for you if you call its internal whatnot) and that requires *writing* zeros to particular TIMx_SR bits (i.e. not RMW!)
> The famous UM1725
Read the sources, Cube/HAL is open source.
Or, way better, ditch Cube entirely and go for adult programming. RM is your friend.
JW
2020-03-17 1:25 AM
HAL functions are rather poorly documented, I could never figure out how these HAL_TIM_ functions are supposed to work.
Using the register interface as documented in the reference manual works without much guesswork.
GPIO setup would of course be different for your board.
2020-03-17 4:27 AM
Many thanks. I search for sources , I don't know where...
And many thanks, really I'm not adult : only 47 year old ( in Hex obviously).
luciano
2020-03-17 4:28 AM
Many thanks. I try ...
Luciano
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.