2023-06-12 5:36 AM
Running v1.12.1 of STM32CubeIDE. I noticed that the OTG SFRs are not showing up for the STM32L475. They do show up for an STM32L476.
Does anyone know how I can fix this? thanks
Solved! Go to Solution.
2023-06-12 4:44 PM
You can use the L476 SVD file instead. Or edit the SVD file to include those registers. ST has a history of mucking up the SVD files.
SFRs window -> Configure SVD settings (wrench icon) -> choose new file
2023-06-12 4:44 PM
You can use the L476 SVD file instead. Or edit the SVD file to include those registers. ST has a history of mucking up the SVD files.
SFRs window -> Configure SVD settings (wrench icon) -> choose new file
2023-06-12 7:25 PM
Thank you very much. This worked for me.
2023-06-13 1:26 AM
Hello @SHuds.1 ,
Thank you for bringing this issue to our attention.
I confirm the issue and I reported internally.
Also I recommend you to refer to this FQ to add or update the SVD file in different toolchains: How to add or update the SVD file in different toolchains: An example using Nucleo-U575ZI-Q board.
Internal ticket number: 154673 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.