2026-03-26 5:25 AM
I'm trying to create an empty project for the NUCLEO-U3C5ZI-Q using STM32CubeIDE v2.1.1 under MacOS. All available updates have been applied.
I've used File/STM32 Project Create to create an STM32CubeIDE Empty Project for the NUCLEO-U3C5ZI-Q board (all settings at the defaults offered).
The project is created, along with the startup and linker files, but there is no .ioc file.
Solved! Go to Solution.
2026-03-26 5:28 AM
STM32CubeIDE v2.0 and later do not create IOC files or STM32 projects. The ability to interact with IOC files has been removed. Use the standalone STM32CubeMX for that.
2026-03-26 5:28 AM
STM32CubeIDE v2.0 and later do not create IOC files or STM32 projects. The ability to interact with IOC files has been removed. Use the standalone STM32CubeMX for that.
2026-03-26 5:41 AM
@TDK wrote:STM32CubeIDE v2.0 and later do not create IOC files or STM32 projects. The ability to interact with IOC files has been removed. Use the standalone STM32CubeMX for that.
Indeed - I was just coming back to say the same thing ;)
2026-03-26 5:45 AM - edited 2026-03-26 5:47 AM
As @TDK said, this was an intentional change in CubeIDE v2.0.0, back in November last year (announced in September):
See: STM32CubeIDE 2.0 release - early heads-up!
And: STM32CubeIDE 2.0.0 released
New tutorial here: STM32CubeIDE 2.0.0 workflow tutorial
Explanation & discussion here: IDE Version 2.0.0 - why remove MX ?
#SeparateMXfromIDE #IDEindependentMX #MXremovedFromIDE
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.