2025-08-19 2:50 AM - last edited on 2025-08-19 4:12 AM by mƎALLEm
stm 32 nucleo -G071RB , TARGET NOT RESPONDING
I am not able to run after dumping the code once i use the run commond after dumping i am getting
arget is not responding, retrying...
Target is not responding, retrying...
Shutting down...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
I tried changing the USB,Workspace,and opened new project still having same issue.
I am using STM32 Cube ide version 1.12.0 and this issue same in the other latest version 1.19.0 and firmware package is STM32Cube FW_GO V1.6.2
2025-08-19 3:15 AM
Hello @divzz
If you are unable to connect to your STM32 Nucleo-G071RB board, try using the "Under Reset" option in STM32CubeProgrammer by selecting it in the reset mode dropdown before connecting. This approach can help establish communication with an unresponsive device. If the issue persists, test the board on another computer to rule out PC-specific issues, and consider the possibility of hardware faults with the Nucleo board.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.