2019-10-21 12:25 AM
Could anybody help me how to do multi core debugging with STM32CubeIDE 1.1.0?
2019-10-22 5:54 AM
I'm working on a document to cover this topic in a bit more detail but it's not done yet. What are you having trouble with?
2019-10-22 6:45 AM
Thanks for your reply. I just can't download the two images. I can one by one. But then the other fails.
2019-10-22 7:56 AM
2019-10-23 4:38 AM
How did you set up the debug configuration? In the "Startup" tab of the two sub-projects you need to make sure to click "Add..." to set up which one(s) you wish to load to the target.
2019-10-23 4:53 AM
I have tried this too in various configurations. I just needs some documentation to be useful. Did True Studio have a similar setup. Is the old documentation available?
2019-10-23 6:01 AM
No, we didn't have it in TrueSTUDIO. All the "multi-core" device support was added just now in 1.1.0 (H7/L5/MP1) and they made a specific new feature for flashing (the Startup tab). The documentation is being made right now but MP1 and L5 has gotten prioritized and will most likely be release first.
But the basics is this, I will only mention a setting if it differs from the default.
CM7 - Debug configuration:
Debugger
Reset behaviour: Connect under reset
Tick Halt all cores
Tick Enable shared ST-LINK
Startup Tab
Add the other project
Untick Load Symbols
CM4 - Debug configuration:
Debugger
Add like +10 or something to the GDBserver (for example 61244)
Reset behaviour: None
Tick Enable shared ST-LINK
Startup Tab
Edit the CM4 project
Untick Download
Then you start to debug the CM7 and after that you launch a second debug session (without terminating CM7) with the CM4.
2019-10-23 6:07 PM
2020-02-18 4:07 AM
hI @Markus GIRDLAND : I assume your document eventually became AN5361
I used that as a starting point, however the M4 often crashes whenever I try to debug it. There have been several other posts about the same issue, but none with a proper answer/solution. Do you know how to how to if a fix/recommended workflow is coming?
I posted a simple blinky to github: https://github.com/AnielShri/H745_Nucleo
2020-02-20 4:29 AM
Yes, that's the document I was working on at the time.
I believe this should be fixed in the next version. It has a lot of quality of life and bug fixes for dual core debugging.
Try that version (should be out in a day or two) and see if it fixes anything, if not then let me know and we'll take a closer look!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.