2024-02-22 4:32 PM
Hello,
Somebody knows if the copyright notice generated at the beginning of main.c file is stored in a file that I can edit?
I read in this forum that sections outside of user code are copyrighted by ST. If the copyright text is stored in an editable file, I would add a copyright or copyleft for the user code sections in this file to save time.
Using CubeIDE 1.13.2 for Linux
Thank you
2024-02-22 4:49 PM - edited 2024-02-22 4:49 PM
The copyright notice generated at the beginning of main.c is surrounded by /* USER CODE BEGIN Header */ /* USER CODE END Header */. The actual usage requirements on Cube-generated files (what license files or texts are required legally): see the generated text itself: Since Cube does not currently create the LICENSE file: provided as-is.
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
2024-02-22 5:13 PM
Previously, on ST Community:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.