2022-08-17 4:39 AM
The 1.8 release notes claim that the wayland support bug was fixed, yet the mcu finder still doesn't work. Please reopen bug 77518 or fix the issue.
2022-08-17 5:48 AM
Hi @AWarr.1 ,
Can you please open the CubeIDE installation folder and right click the file 'stm32cubeide_wayland' and select 'Run as a Program'.
Regards,
Aymen.
2022-08-30 6:43 AM
Hello @AWarr.1
Did the proposition of @Aymen CHAKROUN came to help?
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-30 7:07 AM
As far as I can tell, this executable is only delivered with the generic linux build. I am using the rpm installer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.