2020-02-06 4:10 PM
I am using STM32CubeIDE to generate the code.
The only MAC address that will work is 02:00:00:00:01. This address shows up in
the LWIP\Target\ethernetif.c file in the static (void low_level_init(struct netif *netif) function. If I change it to anything else, the board no longer responds to ping.
In the /* USER CODE BEGIN MACADDRESS */ section I tried assigning another MAC address to the board but the board then doesn't respond to ping. If I assign the MAC address as 02:00:00:00:00:01 in this section it does respond to ping.
There is another reference to MAC addresses at Section 1: Ethernet peripheral configuration in the stm32fxx_hal_conf.h file. This is what displays:
#define MAC_ADDR0 2U
#define MAC_ADDR1 0U
#define MAC_ADDR2 0U
#define MAC_ADDR3 0U
#define MAC_ADDR4 0U
#define MAC_ADDR5 1U
However, I can change the #define statements to anything and is has no affect, the system still answers pings.
Exactly how do you set the MAC address for the board? Since the STM32 doesn't have a unique MAC address I will use a Microchip 11AA02E48 to obtain an address.
2020-02-09 1:46 PM
Further investigation reveals the board will also work with a MAC address of 03:00:00:00:00:01. And reading on Wikipedia indicates that these 2 MAC addresses are locally administered addresses instead of universally administered.
So the question is "Has ST somehow hardcoded something on the Discovery board that prevents you from assigning a MAC address to the board?" I have tried everything I can think of for the last 8 hours to assign another MAC address to the board and can't find a way to do it.
I wanted to test 2 Discovery boards for passing Ethernet packets back and forth between the boards before designing a custom board for my application. My concern now is whether I will be able to assign MAC addresses to the STM32F407 on my custom boards.
Or is the MAC address assigning problem really a STM32CubeIDE bug? Does anyone have any suggestions? I am totally stumped at this point.
2020-02-09 3:25 PM
For a typical configuration to work, eventually the same MAC address must be in two places - in the respective ETH MAC peripheral registers and in netif->hwaddr of lwIP. If that's the case and the address is not conflicting with any other device in your local network, then you have some other problem. But I can assure you that the problem is not in MCU internal hardware or lwIP, but only in ST's software - HAL/CubeMX code. You can see my Ethernet demo to see that I know what I'm talking about. And even more important - see my topic of network issues.
> really a STM32CubeIDE bug?
HAL/CubeMX code is non-working bloatware. It's so broken, that "workarounds" require more work than a complete rewrite from scratch. OK, for F4 series it's not so tragic - it can even be made somewhat working, but it's still buggy and incomplete. For a serious projects in the long term only one thing can be recommended - to drop the HAL/CubeMX code completely and use CubeMX only as a pin selection helper tool, when designing PCB.
2020-02-09 5:44 PM
Piranha, thank you for the reply. I had previously read your two references while trying to solve this problem.
As far as I can tell, the MAC information only shows up in the ethernetif.c file that is in the LWIP->Target directory. In that directory there is a function named
static void low_level_init(struct netif *netif). If I use CubeMX to assign a MAC address of 02:00:00:00:00:01, the code that gets generated is this:
static void low_level_init(struct netif *netif)
{
uint32_t regvalue = 0;
HAL_StatusTypeDef hal_eth_init_status;
/* Init ETH */
uint8_t MACAddr[6] ;
heth.Instance = ETH;
heth.Init.AutoNegotiation = ETH_AUTONEGOTIATION_ENABLE;
heth.Init.PhyAddress = DP83848_PHY_ADDRESS;
MACAddr[0] = 0x02;
MACAddr[1] = 0x00;
MACAddr[2] = 0x00;
MACAddr[3] = 0x00;
MACAddr[4] = 0x00;
MACAddr[5] = 0x01;
heth.Init.MACAddr = &MACAddr[0];
heth.Init.RxMode = ETH_RXPOLLING_MODE;
heth.Init.ChecksumMode = ETH_CHECKSUM_BY_HARDWARE;
heth.Init.MediaInterface = ETH_MEDIA_INTERFACE_RMII;further down in that function this appears:
/* set MAC hardware address */
netif->hwaddr[0] = heth.Init.MACAddr[0];
netif->hwaddr[1] = heth.Init.MACAddr[1];
netif->hwaddr[2] = heth.Init.MACAddr[2];
netif->hwaddr[3] = heth.Init.MACAddr[3];
netif->hwaddr[4] = heth.Init.MACAddr[4];
netif->hwaddr[5] = heth.Init.MACAddr[5];In the stm32f4xx_hal_conf.h file there is this reference to the MAC address:
#define MAC_ADDR0 2U
#define MAC_ADDR1 0U
#define MAC_ADDR2 0U
#define MAC_ADDR3 0U
#define MAC_ADDR4 0U
#define MAC_ADDR5 0Ubut I don't know what they are doing here. I can ping the board with the code shown above.
If I then run CubeMX again and change the MAC address to 00:80:E1:00:00:01 and re-generate the code, I can no longer ping the board.
The static void low_level_init(struct netif *netif) function does show the new MAC address but the #define statements in stm32f4xx_hal_conf.h file do not change.
If I use CubeMX to change the MAC back to 02:00:00:00:00:01 the board then once again responds to pings.
The only place I can find anything about the ETH MAC peripheral resgisters is in the stm32f4xx_hal_conf.h file. Is there somewhere else that the MAC information is stored? It doesn't matter what MAC address I try to use, the only one that works is 02:00:00:00:00:01.
"For a serious projects in the long term only one thing can be recommended - to drop the HAL/CubeMX code completely and use CubeMX only as a pin selection helper tool, when designing PCB." -- That would mean writing all of the STM32 Ethernet code from scratch which could take years. Am I missing something?
EDIT: Piranha, you were right, it was another problem.
I am using a Linux server as my DHCP server. I cleared the DHCP leases from the server and now the STM32 Discovery board will work with a different MAC address. I am not sure what is going on with the DHCP daemon. I also found out the #defines in stm32f4xx_hal_conf.h are not needed. I can comment them out and the board still works. Again, I don't have any idea what ST is doing with those.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.