2025-10-19 1:20 AM
Hi
Recently, when I import an LWIP example project from MDK to CubeIDE, I get the following note message::
"note: the message above does not take linker garbage collection into account"
I have 2 questions against these notes:
1. Do these notes have any negative affects on generatiing correct binary of the project ?
2. If they don't have any negative affects, then how to avoid these annoying messages ?
Thanks
Chao
Solved! Go to Solution.
2025-10-20 2:20 AM
Hello @Chao
I assume that this issue has been answered here: Solved: STM32CubeIDE 1.13.0 problem - Page 3 - STMicroelectronics Community "this is ‘just’ a warning, and the linker is able to generate a proper ELF file. As long as your application does not use read/write/close/lseek (which should be the case for a bare metal application), your application will run properly."
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-20 2:20 AM
Hello @Chao
I assume that this issue has been answered here: Solved: STM32CubeIDE 1.13.0 problem - Page 3 - STMicroelectronics Community "this is ‘just’ a warning, and the linker is able to generate a proper ELF file. As long as your application does not use read/write/close/lseek (which should be the case for a bare metal application), your application will run properly."
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-25 12:58 AM
Thank you so much! I found the syscall.c is missing in my project.
Chao
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.