2020-03-16 2:10 PM
I haven't figured out how to get it to import an example in STM32CubeIDE and compile it. I tried to recreate the project based on one generated with STM32CubeMX, but had no luck.
I eventually tried SW4STM32 and at least got it to compile there, but then when it tries to flash it via openocd it errors out there, but that's a different issue.
2020-03-17 1:16 AM
> I haven't figured out how to get it to import an example in STM32CubeIDE
File > Open Projects from file System...
will automatically convert.
> when it tries to flash it via openocd
Try to create a new debug configuration and use that.
2020-03-17 3:16 AM
MacOSX Mojave
STM32CubeIDE 1.3.0
Empty new workspace.
File -> Open projects from filesystem...
Directory...
STM32Cube_FW_G0_V1.3.0/Projects/NUCLEO-G071RB/Examples/DAC/DAC_SignalsGeneration
It has two items in the table:
DAC_SignalsGeneration Eclipse Project
DAC_SignalsGeneration/SW4STM32/DAC_SignalsGeneration Convert 'System Workbench for STM32' project to STM32CubeIDE project
Both are checked. Click Finish.
Click Debug.
The selection cannot be launched, and there are no recent launches.
Double-click on something in the project explorer. Click on Debug again. Something momentarily pops up and disappears. Nothing seemed to have happened.
In the Project dropdown most things are greyed out, so I don't know where to create a new debug configuration.
Under the run menu, there's a Debug Configurations... item. Clicking on that gives a dialog. In the left there's STM32 Cortex-M C/C++ Application. Double-clicking that gives DAC_SignalsGeneration. Should I do anything else in this dialog?
Then if I close it and hit Debug again I get a dialog that pops up and says 'Launching DAC_SignalsGeneration has encountered a problem'. Clicking on details says:
An internal error occurred during: "Launching DAC_SignalsGeneration".
java.lang.NullPointerException
What am I doing wrong? Is there instructions on how to use STM32CubeIDE somewhere? A getting started guide perhaps?
2020-03-17 4:34 AM
I'm not familiar with Mac, but a general introduction is
2020-10-06 2:43 AM
Did you find a way how to build STM32Cube_FW_Fx project examples in Cube IDE?
2020-10-06 3:08 AM
2020-10-06 4:11 AM
I decided to learn Cube IDE a bit. Just found a reddit thread about similar problem and the answer was shocking - try to double click on .project file.
Well, I tried to exec "c:\Users\user\STM32Cube\Repository\STM32Cube_FW_F3_V1.11.1\Projects\STM32F303RE-Nucleo\Demonstrations\Adafruit_LCD_1_8_SD_Joystick\.project" (I play with Nucleo-F303RE) and Cube IDE started to blame on non existing JRE. After java installation project was successfully imported, built and downloaded.
2021-07-18 1:35 AM
From my experience, the best way to learn the examples is:
This is how I learned timers with interrupts, ADC with DMA, DAC, SPI for display and digital potentiometer, and finally integrated C++ code into C project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.