2023-04-04 8:24 AM
This is likely not a problem with 1080p displays. But on a 32" 4K display, even at 150% scaling, the icons are too small for my glasses prescription. Just look at those icons in my png. I've been digging into the preferences for icon size control, and I'm either looking right at it or it's not in there. And searches through your DB gives no joy. Is there some ini file I need to be editing by hand?
Dave
2023-04-04 9:47 AM
you know this:
2023-04-04 10:24 AM
Thank you very much for the answer AND the new site to pour over. :)
2023-04-04 10:51 AM
+ in eclipse:
>>
worked like a charm for me although I made them 150 %
-Dswt.autoScale=150
and should be repeated this goes in eclipse.ini file
also, the icons look grainy , but at least they are bigger
<<
see:
https://www.eclipse.org/forums/index.php/t/1088764/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.