2024-04-11 2:34 AM - edited 2024-04-11 2:43 AM
IS stm32f401re will support with LoRa993 will it commutate ?
Solved! Go to Solution.
2024-04-11 2:42 AM
You're the second person this week asking about this.
Give the full part number and link to the data sheet or manual.
You should be able to connect up power and an UART connection.
Perhaps use a USB to CMOS Serial adapter and communicate with it from a PC Terminal application until you're comfortable with how the interaction with the module is expected to behave.
2024-04-11 2:41 AM
@sumant1 wrote:LoRa993
A what?
Do you mean this: https://reyax.com/products/RYLR993 ?
(please always give a link so that we can see exactly what you're referring to)
If so, see this recent thread:
https://community.st.com/t5/stm32cubeide-mcus/how-to-interface-lora-993-with-stm32f401re/m-p/657669
and duplicate:
2024-04-11 2:42 AM
You're the second person this week asking about this.
Give the full part number and link to the data sheet or manual.
You should be able to connect up power and an UART connection.
Perhaps use a USB to CMOS Serial adapter and communicate with it from a PC Terminal application until you're comfortable with how the interaction with the module is expected to behave.
2024-04-11 2:46 AM
Is this a school project?
Have your supervisor or professor GUIDE you and your colleague. Kinda his job..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.