2023-11-17 2:23 PM
Hello,
I am installing STM32CubeIDE on Linux (Ubuntu) and have several challenges where when I am importing the BSP to the repository, it hangs and will now allow me to finish. I believe it is trying to retrieve the file but gets hung up because I may not have signed in beforehand. However, I get the attached error when I reinstalled it - and really would like to know what it means opposed to choosing yes/no. Does somebody want to comment or know? Thank you so much.
2023-11-17 5:28 PM - edited 2023-11-17 5:31 PM
You normally don't open .project & .cproject files directly from Nautilus etc. - there's a reason why these files are hidden. You open Eclipse projects in the Eclipse GUI by importing them or creating. To import a project as is, or convert from other format, use the IDE File->Import.
So normally there's no need to associate .project & .cproject files with anything at all. No is a safe answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.