2022-07-02 3:40 PM
Example is the LwIP_HTTP_Server_Netconn_RTOS project
step 1 Create one from the examples.
Step 2 Note the directory structure
./LwIP_HTTP_Server_Netconn_RTOS is the top most directory
There are SRC files located here:
./LwIP_HTTP_Server_Netconn/src
The .project file is located here:
./LwIP_HTTP_Server_Netconn/SW4STM32/STM32H743ZI_Nucleo/.project (and .cproject)
I wish to add a new source level directory up at the top, example:
./LwIP_HTTP_Server_Netconn/src_two
The tool only allows me to make or add things at or below the .project file
why?
Steps to reproduce:
Choose: FILE -> New -> Source Folder
Click: "browse" - it is not possible to move UP to the top level project where SRC is located
I cannot type: ../src - as a relative path - that does not work either
The directory *MUST* be at or below the .project folder.
2022-07-02 6:52 PM
Read on "Link a source folder".
Linked folders and files are feature of Eclipse, not specific to CubeIDE.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.