2021-01-13 10:42 AM
Hello guys!
I am now using stm32cubeide and the issue is that there are 2 headers and I need them to include each other but when I do that, the compiler indicates that my typedef struct defined in a header is conflicting types. I have used this preprocess syntax for each header:
"
#indef _Header_H_
#define _Header_H_
#endif
"
but it's not working. Does anyone know how to solve this?
2021-01-13 11:19 AM
Exactly like with every other IDE, compiler and googleplex examples in the Internet... Obviously #endif must be at the end of the file.
Also take a look on this:
https://stackoverflow.com/questions/1143936/pragma-once-vs-include-guards
https://stackoverflow.com/questions/787533/is-pragma-once-a-safe-include-guard
2021-06-23 11:41 AM
Hi, I have same error
I include a header file in several .c files
it gives error - multiple definition
I tried to make an "include guard" as below
however multiple definiton error again
CubeIDE gcc STM32F103
please advice , thanks
#ifndef INC_US_GLOBAL_H_
#define INC_US_GLOBAL_H_
uint8_t RAM[0x1e00],RLO;
int16_t ACCU1 , ACCU2 , PARAM1,ikl=0;
uint8_t TIMERSTART[128], TIMEROUT[128];uint16_t TIMERSET[128];
unsigned char toggle, toggleLED=1,pai;
.............
uint8_t Rx_buffer[512], Rx_buffer_3[20];
volatile uint8_t TIMERJOB, Tx_buffer_2[512];
volatile int16_t Rx_ptr_2,counterhi;//ADCresult;
#endif // INC_US_GLOBAL_H_
2021-06-23 12:21 PM
Perhaps stop defining things in .H files, keep that in ONE .C file, and use extern in the .H files!!
2021-06-23 12:23 PM
Don't Do This!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.