2020-04-14 1:12 AM
I'm controlling the temperature of high power heaters in my project. Because ithe product can damage if the heaters stay on too long, I have added code to disable the heaters in the hard fault handler. This way I can be sure that if something goes wrong the heaters are turned off directly.
However, it turns out that if the hard fault handler is entered while debugging a breakpoint is set at the beginning of the handler. All safety code that follows after the breakpoint isn't executed until I continue the program.
Since the heaters can overheat in a few seconds there is a good chance I'm not fast enough to respond when this happens. Can anyone tell me how I can make STM32CubeIDE not stop there or not add breakpoints at the hard fault handler?
Solved! Go to Solution.
2020-04-14 1:35 AM
Open the Run / Debug configurations dialog, uncheck Halt on exception on the Startup tab. You may have to scroll down to expose the option.
2020-04-14 1:35 AM
Open the Run / Debug configurations dialog, uncheck Halt on exception on the Startup tab. You may have to scroll down to expose the option.
2020-04-14 3:06 AM
Thank you so much!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.