2020-12-05 8:52 AM
I purchased STM32H757I-EVAL board and after installing STM32CUBE 1.5, and STM32CubeH7 Firmware Package V1.8.0 / 29-May-2020, I dont see GPIO_EXTI example listed for STM32H757I-EVAL or STM32H747I-EVAL in "Import STM32Cube Example". The directory Projects\STM32H747I-EVAL\Examples\GPIO\GPIO_EXTI exists in the installed Firmware Package. How can I try out a simple example. Am struggling for 2 days now!!!!
2020-12-09 11:10 PM
Hello @[SS.11] ,
Welcome to the STM32 Community :smiling_face_with_smiling_eyes:.
You can run the GPIO example available under STM32Cube_FW_H7_V1.8.0\Projects\STM32H747I-EVAL\Examples\GPIO\GPIO_EXTI.
This example runs on STM32H757xx devices and be ure to follow the instructions in the readme file
You can select the suitable IDE for you: EWARM, MDK, SW4STM32, or migrate the project to STM32CubeIDE following the user manual to import Cube projects from SW4STM32 or TrueSTUDIO to STM32CubeIDE:
Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.