2026-01-14 6:24 PM
I recently upgraded my IDE to version 2.0. I cannot start a project from the board view; where you select the board type and configure the settings. It would then create the c++ project code for you. The new version doesn't have anything to help you select the board and it cannot even open up the board configuration editor when you click on the .ioc file. Is there. a way to revert back to the previous editor version - I think it was version 1.x.18?
Solved! Go to Solution.
2026-01-14 11:45 PM
Hello @dshenoy
In the latest release , STM32CubeMX is no more integrated in STM32CubeIDE 2.0.0
For more details , please check this STM32CubeIDE 2.0.0 released
To download CubeMX standalone please use this LINK
See: STM32CubeIDE 2.0.0 New workflow tutorial
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-14 7:27 PM
Uninstall that version, download the previous version and install it.
STM32CubeIDE | Software - STMicroelectronics
Or use STM32CubeMX in standalone mode as intended.
2026-01-14 11:45 PM
Hello @dshenoy
In the latest release , STM32CubeMX is no more integrated in STM32CubeIDE 2.0.0
For more details , please check this STM32CubeIDE 2.0.0 released
To download CubeMX standalone please use this LINK
See: STM32CubeIDE 2.0.0 New workflow tutorial
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.