2022-03-29 12:54 AM
Is there a plugin Git (for version 2.19.1 and 2.27.0) in .tgz that I can install in /applis/STM32CubeIDE_1.5.0 directory ?
Thanks
2022-03-29 6:13 AM
Typically git is installed at the system level and included in the system path, not in a target directory.
2022-03-29 7:59 AM
Yes , Git is a application installed outside STM32CubeIDE installation but the plugin for using Git must be installed in /applis/STM32CubdeIDE no ?
Thanks
2022-03-31 12:57 AM
The STM32CubeIDE is based on eclipse 4.16.0 . Is a plugin Git for eclipse 4.16.0 will run in the /applis/STM32CubeIDE_1.5.0 installation ?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.