cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_I2C_Mem_Read_IT

VPICINC
Associate

I'm using the Nucleo-G491RE board, and the STM43G491VET chip. The call to HAL_I2C_Mem_Read_IT works on the chip, but not on the Necleo board. The .ioc is the same for both, but the Nucleo says HAL is busy if you go into the HAL code. Both are using a 68 MHz system clock. Any idea why they would act different?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

If the code is the same, differences in hardware are probably causing the differences in behavior.

If you feel a post has answered your question, please click "Accept as Solution".
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.