2021-03-03 1:56 AM
Hi
I would like to get buildnumber in stm32 controller and using STM32 cube ide. I can get date and time but not build number. Any suggestions.
__BUILD__,__DATE__,__TIME__I am getting error on getting buildnumber using __BUILD__.
Any suggestions on how to get it??
2021-03-03 5:19 AM
Is __BUILD__ supported ? Predefined Macros (The C Preprocessor) (gnu.org)
Maybe have you to build such by your own (based on some PID or ..). Found such which may be interesting: How to store compilation date in the final binary file in order to read it by an external program?
2021-03-03 5:34 AM
Don't know CubeIDE.
But all modern toolchains have an option to define pre- and post build steps, so one can run e.g. a script to generate those defines with incrementing numbers.
The simplest way is a separate header where you edit the defines manually.
2021-03-03 6:53 AM
Pre & post build are STM32CubeIDE supported for sure.
2021-03-03 7:25 AM
Post build is useful for other tasks.
My company uses our own bootloader in a safety environment, so we patch data like checksums into the S19 file after the build.
2021-03-03 8:00 AM
Would your "build" be your repository version, or are you aiming for something else?
The Keywords __DATE__,__TIME__ are from the compiler, which has no idea what change history you have.
If you are using TortoiseSVN you can under settings set it to run a script when committing, and in TortoiseSVN you can flag a file generated by the script to have select fields updated as part of the commit.
For a group it might be better to put the script on the SVN server to be automatically run for all commits to the repository, it could be similar and create a set of #define accessible in your code.
I just did this Monday: SvnVersion_V01_20210301PR.zip.
Will need a "mid string" function to extract version, and best convert to a numeric to discard any leading spaces.
Paul
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.