2022-08-02 11:11 PM
FP-CLD-AWS1 software package v3.0.1 for STWINKT1B fails to be compiled in higher STM32CubeIDE version than 1.8.0. Library link error happens. It is successfully compiled only in 1.8.0. version. It seems to be IDE bug.
I hope it to be checked and fixed.
Solved! Go to Solution.
2022-08-05 7:19 AM
2022-08-03 8:01 AM
Exactly what errors are you getting?
The IDE changed compiler versions somewhere in the 1.8/1.9/1.10 releases, I don't recall exactly which one. And the newer compiler versions change some default compiler/linker settings. One that got a lot of attention on this forum was the change to how the linker handled "multiple definitions" of variables. Lots of sloppy code would put "int somevar" in the include file instead of "extern int somevar". With the old default "-fcommon" setting, the linker would merge all of those into a single instance. The newer default "-fno-common" does not merge them and you get dozens/hindreds of "multiple definition" errors from the linker.
2022-08-03 9:34 PM
Copied and pasted error I am getting.
[CubeIDE 1.8.0]
arm-none-eabi-gcc -z max-page-size=0x200 -o "STWINv1_aws_demos.elf" @"objects.list" -l:se_interface_app.o -mcpu=cortex-m4 -T"D:\3View\AWS\STM32CubeFunctionPack_AWS1_V3.0.1\Projects\STEVAL-STWINKT1\Applications\Cloud\aws_demos\STM32CubeIDE\STM32L4R9xx_FLASH_sbsfu.ld" --specs=nosys.specs -Wl,-Map="STWINv1_aws_demos.map" -Wl,--gc-sections -static -L../../../../BootLoader_STSAFE/2_Images_SBSFU/STM32CubeIDE/STWINv1_2_Images_SBSFU/Debug -Xlinker -L ../../../../BootLoader_STSAFE/Linker_Common/STM32CubeIDE -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -u _printf_float -u _scanf_float -Wl,--start-group -lc -lm -Wl,--end-group
Finished building target: STWINv1_aws_demos.elf
arm-none-eabi-size STWINv1_aws_demos.elf
arm-none-eabi-objdump -h -S STWINv1_aws_demos.elf > "STWINv1_aws_demos.list"
arm-none-eabi-objcopy -O binary STWINv1_aws_demos.elf "STWINv1_aws_demos.bin"
text data bss dec hex filename
377808 3584 383824 765216 bad20 STWINv1_aws_demos.elf
Finished building: default.size.stdout
Finished building: STWINv1_aws_demos.bin
Finished building: STWINv1_aws_demos.list
"../../../../BootLoader_STSAFE/2_Images_SECoreBin/STM32CubeIDE/postbuild.sh" ".." "./STWINv1_aws_demos.elf" "./STWINv1_aws_demos.bin" "1" "bigelf"
prepareimage with windows executeable
Generating the global elf file (SBSFU and userApp)
[CubeIDE 1.9.0 & 1.10.1]
arm-none-eabi-gcc -z max-page-size=0x200 -o "STWINv1_aws_demos.elf" @"objects.list" -l:se_interface_app.o -mcpu=cortex-m4 -T"D:\3View\AWS\STM32CubeFunctionPack_AWS1_V3.0.1\Projects\STEVAL-STWINKT1\Applications\Cloud\aws_demos\STM32CubeIDE\STM32L4R9xx_FLASH_sbsfu.ld" --specs=nosys.specs -Wl,-Map="STWINv1_aws_demos.map" -Wl,--gc-sections -static -L../../../../BootLoader_STSAFE/2_Images_SBSFU/STM32CubeIDE/STWINv1_2_Images_SBSFU/Debug -Xlinker -L ../../../../BootLoader_STSAFE/Linker_Common/STM32CubeIDE -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -u _printf_float -u _scanf_float -Wl,--start-group -lc -lm -Wl,--end-group
c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: cannot use executable file '../../../../BootLoader_STSAFE/2_Images_SBSFU/STM32CubeIDE/STWINv1_2_Images_SBSFU/Debug\se_interface_app.o' as input to a link
collect2.exe: error: ld returned 1 exit status
make[1]: *** [makefile:104: STWINv1_aws_demos.elf] Error 1
Can you tell me how to change linker or compiler default setting in CubeIDE?
Regards,
Ernest
2022-08-05 7:19 AM
2022-08-08 3:20 AM
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.