2022-07-07 4:33 AM
Hello,
I am trying to compile code that works fine on my friend's pc.
the problem is that I am keep getting error that the compiler can't find the "stm32f7xx_hal.h" file even dough its there and I added it to the include paths.
can someone help?
2022-07-07 2:41 PM
Check the compiler options in the build console view for the correct -I includes.
Check for spaces or other non-trivial or non-ASCII characters in the path like umlauts, quotes, ...
hth
KnarfB
2022-07-07 5:23 PM
I'm not an Eclipse/CubeIDE adherent, but is a "Project Tree" actually a directory? Will the file load into the IDE if you click on it? What path does that show?
Show me this in a File Manager.
Make sure that whatever environment variable expansion you have in your Include Paths list actually expands to what you think it does.
2022-07-08 3:01 AM
@Community member "is a 'Project Tree' actually a directory?"
No, it isn't.
"Will the file load into the IDE if you click on it? What path does that show?"
+1
"Show me this in a File Manager"
+1
"Make sure that whatever environment variable expansion you have in your Include Paths list actually expands to what you think it does."
+1
The screenshot shows workspace_loc and ProjName used - so check that they are actually pointing to the correct places...
And, as @KnarfB said, check for "weird" characters in file (including folder) names;
2022-07-12 10:57 PM
2022-07-13 1:01 AM
and are you sure that folder matches your Include paths - after the symbols are expanded?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.