2020-05-15 9:56 AM
I'm working in STM32 CubeIDE with a Blue Pill board.
To control the size of main.c I have gathered groups of functions together in to several c/h pair files. One of the pairs is 'myirqcallbacks.c/h". At the moment I have two UART IRQs and an external pin IRQ callback in this c/h pair.
The UARTs work fine but the EXT IRQ fails to call my code. It runs the __weak copy in stm32f1xx_hal_gpio.c instead.
When the code was in main.c it ran OK.
It seems that the compiler can't see my EXT IRQ callback function so fails to deprecate the __weak copy of the callback. It can however see the two UART callback functions in there. Is there some difference in the structure of the GPIO and UART IRQs?
myirqcallbacks.h
/*
* myirqcallbacks.h
*
* Created on: 13 May 2020
* Author: Paul
*/
#ifndef SRC_MYIRQCALLBACKS_H_
#define SRC_MYIRQCALLBACKS_H_
void HAL_GPIO_EXT1_Callback ( uint16_t GPIO_Pin); // SIM Reset detected
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart); // Outgoing debug, control and up-the-line data.
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) ; // Data from SIM
#endif /* SRC_MYIRQCALLBACKS_H_ */myirqcallbacks.c
* myirqcallbacks.c
*
* Created on: 13 May 2020
* Author: Paul
*/
#include <circbuf.h>
#include "main.h"
#include "stdio.h"
#include "myfuncs.h"
#include "myirqcallbacks.h"
#include "globals.h"
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart) // Outgoing debug, control and up-the-line data.
{
if( huart->Instance == huart1.Instance)
{
if( buf_tx1.count > 0)
{
uint8_t item;
cb_pop_front(&buf_tx1, &item );
if(HAL_UART_Transmit_IT(&huart1, &item, 1 )!= HAL_OK)
Error_Handler();
}
}
__NOP();// Check all data sent
}
//HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
void HAL_GPIO_EXT1_Callback ( uint16_t GPIO_Pin) //Reset UICC detected
{
if( GPIO_Pin == SIM_RST_Pin)
{
HAL_NVIC_ClearPendingIRQ(GPIO_Pin);
SIMState= SIM_STATE_ATR;
SIM_ATR_Processing = 1;
SIM_ATR_BytesExpected = 2; // +last byte will always be TK (CheckByte)
SIM_ATR_COUNT = 0;
debug("\nSIM-Reset! Proc. ATR\n");
}
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) // Data from SIM
{
if( huart->Instance == huart2.Instance)
{
uint8_t item;
if(HAL_UART_Receive_IT(&huart2, &item, 1)!=HAL_OK)
Error_Handler();
//cb_push_back(&buf_rx2, &item); // Still need to send this up the line, just using local copy to set speed and to debug
if(SIM_ATR_Processing)
processATRByte(item);
}
__NOP();// Check all data received
}I'm thinking this is more about my flaky c file structure knowledge than anything else but I've been on it for a couple of days now and any pointers would be very much appreciated.
2020-05-15 10:32 AM
Check the spelling of the name of the functions.
2020-05-16 1:32 PM
Thanks berendi. Another pair of eyes is a wonderful thing.
2020-05-18 3:46 AM
berendi spotted the error in the function names for which thank you. Sadly this didn't solve the problem, I must have generated this one in my flapping about trying to solve the main problem.
What fixed it in the end was regenerating the code from the MX configurator, which rebuilds the stm32F1xx_hal_gpio.c/h and stm32F1xx_hal_gpio.ex.c/h files. I deleted the local copies first. I found this solution by tracing the path through the equivalent _hal-uart_ files playing spot the difference.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.