2020-06-16 6:33 AM
Hi,
I work with STM32CubeIDE
Version: 1.3.1
Build: 6291_20200406_0752 (UTC)
I somehow managed to disable automatic code generation for altered *.ioc file.
Now it doesn't automatically regenerate the source files according to the changes
I made in the configuration window for my STM32... instead it just shows a bracketed text
besides my *.ioc file in the Project Explorer so I have to click on the "Device Configuration Tool Code Gerneration" button to generate it.
If I remember correctly there was once a question if I want to auto-generate the code.
It seems I denied the question and ticked the "do not ask again" field. How can I revoke that decision?
Solved! Go to Solution.
2020-06-19 5:52 AM
You can revoke your decision relying on Windows>Preferences>STM32Cube>Device Configuration Tool.
By the way asking for code generation if .ioc editor active if possible either relying on Project>Generate code or pushing gear wheel in the toolbar.
2020-06-19 5:52 AM
You can revoke your decision relying on Windows>Preferences>STM32Cube>Device Configuration Tool.
By the way asking for code generation if .ioc editor active if possible either relying on Project>Generate code or pushing gear wheel in the toolbar.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.