2024-06-28 11:06 AM
As per subject. I can see the tasks but it would be most useful if I can see queue status as a USB task isn't always responsive, and mouse movements are discarded if the queue is full.
I have added the 12 or so queues into the registry with the vQueueAddToRegistry() function but they are still not visible.
configUSE_TRACE_FACILITY is defined as "1".
Clearly I am missing something but it's not obvious what?
2024-06-29 12:52 PM - edited 2024-06-29 12:54 PM
Which version?
2024-06-30 5:05 AM
Many thanks.
I’m using STM32CubeIDE version 1.15.1
And using STM32CubeMx version 6.11.1
Libraries STM32Cubde FW_4 V1.28.0
FreeRTOS Version 10.3.1
CMIS-RTOS version 2.00
To my knowledge all version are up to date BICBW
The Task window works well, and I even have the Task utilisation percentages. But getting the Queues to work has beaten me.
2024-07-06 6:11 AM
Can anyone make any suggestions where else I can ask this question for a solution?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.