2024-02-05 10:46 AM
Start a project with FreeRTOS. (default settings_
Change your mind and select emDOS. (default settings)
build project and get missing variables. Decide that bug for emDOS is not yet fixed.
deselect emDOS
Select FreeRTOS instead.
build project (basic, change nothing, do nothing to default settings)
Description Resource Path Location Type
Get following error:
cannot find -l:libosT8MLVHLDT.a: No such file or directory U5_TFT_ILI C/C++ Problem
Problem can be worked around by changing included libraries in project settings.
Any change to the IOC file and subsequent regeneration of code puts the library back in again.
IOC file attached
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.