cancel
Showing results for 
Search instead for 
Did you mean: 

Description Resource Path Location Type Unknown referenced nature: fr.ac6.mcu.ide.core.MCUProjectNature. .project /bootloader Unknown Unknown nature Facing this error as attached.

SUpen.1
Associate II

0693W00000WISbxQAH.png0693W00000WIScHQAX.pngKindly help.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Bob S
Super User

That is a warning, not an error.

Does the IDE build the bootloader if you modify one of the source files? What if you do a "clean" and build? Or do you always get the "nothing to build" message. If the bootloader DOES build when it supposed to, then perhaps just ignore the warning (not an ideal solution).

Which IDE is this? System Workbench? Or CubeIDE on a project imported from System Workbench?

I will not be much help, but that may give people with more in-depth Eclipse knowledge the info they need to help you.

SUpen.1
Associate II

I cleaned the project. Still getting this warning.

This is on stmcubeIDE version 1.9.0.

Is this a SW4STM32 project? If yes, convert it (import) to CubeIDE format.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.