2025-12-08 5:30 AM - last edited on 2025-12-09 10:27 AM by Andrew Neil
Hi, I have a problem with my CubeIDE installation that is that I cannot create a stm32 project(the option that integrates with CubeMX) I can only create the following
I've installed it from the shell script from the generic Linux download, I'm using arch Linux(btw).
I've reinstalled it at least 3 times now, also went to Help -> Install New Software, used this site:
And installed everything down the STM32CubeIDE section.
Solved! Go to Solution.
2025-12-08 5:43 AM
CubeMX is no longer integrated into STM32CubeIDE. To create a new project, download, install and use the standalone STM32CubeMX application.
2025-12-08 5:43 AM
CubeMX is no longer integrated into STM32CubeIDE. To create a new project, download, install and use the standalone STM32CubeMX application.
2025-12-09 10:27 AM
As @TDK said, It's intentional: CubeIDE no longer integrates the MX functionality - it's now only available in the separate, standalone application.
Discussion about this here: IDE Version 2.0.0 - why remove MX ?
2026-01-03 10:48 PM - edited 2026-01-03 10:49 PM
I was horrified from 4 hours. Thanks.
noob googler help:
IOC file not working
cube ide project not opening
cube ide no new project option
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.